• No : 21643
  • Release Date : 2018/08/22 16:28
  • Print

Encoder signal output

Is it possible to output the encoder signal?
Category : 

Answer

It can be output by attaching the plug-in option FR-VPA, FR-VPB, or FR-VPC.
Note that the output format depends on the option type.
FR-VPA: Open collector output (phases A, B, and Z)FR-VPB: Line driver output (phases A, B, and Z)FR-VPC: Line driver output (phases A and B only)Also, note that a divided signal cannot be output.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200