• No : 21657
  • Release Date : 2018/08/22 16:28
  • Print

Model configuration

What types are available?
Category : 

Answer

12 models of FREQROL-V200 vector inverters each for the 200 V and 400 V classes from 1.5K to 45K.
9 models of SF-VR vector control dedicated motors each for the 200 V and 400 V classes from 5.5 to 45K. (55K or higher capacity is supported by the MELTRAC-V200 series.) (55K or higher capacity is supported by the MELTRAC-V200 series.)
Product Name
Inverter, magnet motor drive
Series
FR-V200