• No : 21659
  • Release Date : 2018/08/22 16:28
  • Print

Difference from general-purpose inverter

What are the differences from the general-purpose inverter?
Category : 

Answer

While the inverter uses open-loop (V/F) control, it uses semi-closed loop vector control (constant current control).
This enables output of stable torque especially at low speed, extends the speed control range (1:500), and allows for torque control.
It also enables positioning operation using an option.
You need a vector control dedicated motor or a standard motor with an encoder for vector control.
(An encoder is necessary.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200