- No : 21715
- Release Date : 2018/08/22 16:29
-
Print
Monitor indicator
I set the rotations per minute to Pr.37 (Speed display). Can I check the accumulated number of rotations on the monitor?
- Category :
-
Answer
No. You cannot check the accumulated number of rotations on the monitor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700