• No : 21726
  • Release Date : 2018/08/22 16:29
  • Print

Tuning

Although I set parameters for auto tuning, tuning was not performed and the motor rotated as usual.
How can I perform tuning?
Category : 

Answer

Check the parameters listed below necessary for tuning again.

Pr.9, Pr.71, Pr.80, Pr.81, Pr.83, Pr.84, and Pr.96
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700