• No : 21733
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

I perform remote operation by setting Pr.59 (remote function selection). When the acceleration signal (RH) is turned ON, the frequency rises. Is this frequency stored in any parameter?  
Category : 

Answer

It is not stored in a parameter but memorized as the frequency setting value after acceleration by the acceleration signal.

You can also choose whether or not to clear this frequency setting value when the power is turned off.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700