- No : 21734
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
Can I change Pr.1 (Maximum frequency) during operation?
- Category :
-
Answer
No. You cannot change the setting during operation.
However, setting Pr.77 (Parameter write selection) to "2" allows for the setting change during operation. (Note that changing other parameters is also allowed.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700