• No : 21755
  • Release Date : 2018/08/22 16:29
  • Print

Advanced magnetic flux vector control

I want to operate the inverter using Advanced magnetic flux vector control.
What setting is required?
Category : 

Answer

To use Advanced magnetic flux vector control, basically set Pr.9, Pr.80, Pr.81, Pr.71, and Pr.800.
Auto tuning is necessary in some cases. Set Pr.83, Pr.84, and Pr.96 in addition to above for it.
Set these parameters and perform tuning.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700