- No : 21756
- Release Date : 2018/08/22 16:29
-
Print
Advanced magnetic flux vector control
I want to perform Advanced magnetic flux vector control using the geared motor GM-S(B).
Which value should I set to Pr.71 (Applied Motor)?
- Category :
-
Answer
When using the geared motor GM-S(B), set Pr.71 to "13" and also set Pr.9, Pr.80, and Pr.81.
Perform auto tuning as required. Perform auto tuning as required. Settings of Pr.83, Pr.84, Pr.96, and Pr.800 are also required to be configured.
Set these parameters and perform tuning.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700