• No : 21801
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

I set the frequency to 10 Hz because I wanted to operate the motor at 10 Hz.
When I started the inverter in Advanced magnetic flux vector control, a frequency 10 Hz higher than the setting was output. What is wrong with the inverter setting?
Category : 

Answer

When running the inverter in Advanced magnetic flux vector control, the frequency setting value is increased by the amount of the motor's slippage, resulting in a higher frequency than commanded. It is not a fault.  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700