• No : 21805
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

Which parameter is used to set the maximum frequency when setting the frequency with the setting dial?  
Category : 

Answer

Pr.1 (Maximum frequency) or Pr.18 (High speed maximum frequency).  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700