- No : 21807
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
I use the CC-Link option FR-A7NC to set the frequency to 60 Hz, but the monitor value is shown as "60.09 Hz" when the inverter operates.
Can I adjust it to 60 Hz?
- Category :
-
Answer
Since the Advanced magnetic flux vector control method uses slip compensation to compensate the frequency, the value is not shown as exactly 60 Hz.
For V/F control, check if slip compensation is enabled.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700