• No : 21819
  • Release Date : 2018/08/22 16:29
  • Print

Operation stop, frequency setting

The inverter does not operate.
I want to stop operation and set frequency with the inverter alone.
Category : 

Answer

Set Pr.79 (Operation mode) to "1" (PU operation mode). 
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700