- No : 21832
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
Is there any option to display the operation status during CC-Link operation?
For the FR-E500, the operation panel was removable and I used it.
Should I use the PU connector for connection?
- Category :
-
Answer
You can use optional items, such as enclosure surface operation panel FR-PA07 and parameter unit FR-PU07.
Use the PU connector of the inverter for connection.
Note that you can use the FR-PA02 supplied with the FR-E500 for the FR-E700.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700