• No : 21835
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

By attaching the CC-Link optional card FR-A7NC E kit, how long does the depth of the inverter increase? 
Category : 

Answer

By attaching the optional card and dedicated cover, the depth increases by approximately 15 mm for the FR-E700, and approximately 22 mm for the FR-E700-SC.

Since the terminal block protrudes from the front cover, the depth further increases by approximately 2 mm (2.8 mm at the maximum).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700