• No : 21836
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

I am considering to use the CC-Link option FR-A7NC to operate the FR-E700. Can I use the CC-Link type programming example for the FR-E500 as a reference?
Are there any other good example programs on the Mitsubishi Electric FA Global Website?
Category : 

Answer

You can use the CC-Link type programming example for the FR-E500 as a reference.

In the programming example for the FR-E500, the A series programmable controller is used.
The Instruction Manual of the FR-A7NC provides a programing example for the Q series programmable controller.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700