- No : 21846
- Release Date : 2018/08/22 16:29
-
Print
Setting dial
Can I use the setting dial of the inverter to set the frequency as well as change the parameter values?
- Category :
-
Answer
Yes. You can use the setting dial of the inverter to set the frequency as well as change the parameter values.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700