• No : 21847
  • Release Date : 2018/08/22 16:29
  • Print

FR-E700

I am considering to use the operation panel FR-PA02 for the FR-E500 by connecting it to the inverter with a cable. With the FR-E500, I used Pr.923 (Built-in frequency setting potentiometer gain) to calibrate the frequency setting of the built-in potentiometer. Which parameter should I use for the FR-E700?   
Category : 

Answer

Use Pr.C24 (Frequency setting voltage gain frequency built-in potentiometer).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700