- No : 21854
- Release Date : 2018/08/22 16:29
-
Print
FR-DU07
Can I use the operation panel FR-DU07 that is supplied with the FR-F700 with the FR-E700, FR-D700, or FR-F700PJ?
- Category :
-
Answer
The FR-DU07 cannot be used with the FR-E700, FR-D700, or FR-F700PJ.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ