- No : 21857
- Release Date : 2018/08/22 16:29
-
Print
FR-E700
I want to replace the FR-E500 with the FR-E700.
Is the operation panel of the FR-E700 is detachable like that of the FR-E500?
- Category :
-
Answer
The operation panel of the FR-E700 is not detachable because it is integrated.
The operation panel of the FR-E500 can be used with the FR-E700 by using the connection cable and back cover adapter set.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700