• No : 21860
  • Release Date : 2018/08/22 16:29
  • Print

Operation panel for FR-E500

Can I use the operation panel for the FR-E500 with the E700, D700, or F700PJ?
What is necessary to do this?
Category : 

Answer

The operation panel FR-PA02 for the FR-E500 can be used for these models.
You need the FR-E5P (back cover adapter set) and FR-C20□ (connection cable) for the operation panel.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ