• No : 21862
  • Release Date : 2018/08/22 16:29
  • Print

FR-PA02 built-in potentiometer

How should I configure the setting to use the built-in potentiometer of the operation panel FR-PA02 for the FR-E500?  
Category : 

Answer

Change Pr.146 (Built-in potentiometer switching) to "0" (built-in frequency setting potentiometer).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ