- No : 21890
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
I use 32 input signals containing reserved bits. Since TO command is used to batch write the input signals from the FR-A7NC, 0 is written to each reserved bits. Is it OK?
- Category :
-
Answer
No problem. The inverter actually occupies the reserved bits and does not use them.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700