• No : 21891
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

I use multiple inverters in CC-Link communication, and the "L.RUN" LED on the optional board does not turn on.
How can I check for the cause?
Category : 

Answer

Check if the CC-Link wires are short-circuited and/or station numbers are duplicated.  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700