• No : 21903
  • Release Date : 2018/08/22 16:30
  • Print

CC-Link

I connected the inverter via CC-Link but the "NET" LED on the inverter's operation panel does not turn on.
How can I turn it on?
Category : 

Answer

Set Pr.340 (Communication startup mode selection) to other than "0".
Also, set Pr.79 (Operation mode) to "0", "2", or "6".
Powering the inverter on automatically puts it in the NET mode and "NET" on the operation panel turns on.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700