• No : 21912
  • Release Date : 2018/08/22 16:30
  • Print

Frequency setting

Does using a frequency setting potentiometer of 2 kΩ affect inverter operation?  
Category : 

Answer

You can use it for inverter operation, but the running speed of the inverter does not change linearly with regard to turn of the frequency setting potentiometer.  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700