• No : 21917
  • Release Date : 2018/08/22 16:30
  • Print

Frequency setting

Can I control six inverters with a single external frequency setting potentiometer (potentiometer) simultaneously?  
Category : 

Answer

You can connect up to three inverters to a single external frequency setting potentiometer to control them.  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700