- No : 21918
- Release Date : 2018/08/22 16:30
-
Print
Frequency setting
While the FR-E500 has a built-in potentiometer on the operation panel to set the frequency, the FR-E700 has the setting dial only. How can I set the frequency?
- Category :
-
Answer
Use the setting dial to set the frequency with the FR-E700.
You can also use the setting dial to set the parameters.
(By setting Pr.161, you can use the setting dial as a potentiometer.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700