• No : 21937
  • Release Date : 2018/08/22 16:30
  • Print

Coasting to stop method

How can I perform coasting to stop with the combination of the FR-V200 and dedicated motor?
According to description in the manual, the FR-V200 does not have the terminal MRS.
Category : 

Answer

Use Pr.17 (Input terminal assignment) to assign MRS to the terminals DI1, DI2, and DI3.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200