• No : 21943
  • Release Date : 2018/08/22 16:30
  • Print

Applied motor selection

Pr.71 (Applied motor selection) is set according to the load connected to the inverter. What happens if, for example, I choose the standard motor while the Mitsubishi constant-torque motor is connected?
Category : 

Answer

As the motor operates with the electronic thermal O/L relay characteristics for the standard motor, the thermal error occurs if the motor continuously operates at low speed operation under 100% load.
It means that you are using the constant-torque motor at lower performance. Select the correct motor type with Pr.71.
Product Name
Inverter, magnet motor drive
Series
Others