- No : 22025
- Release Date : 2018/08/22 16:30
-
Print
Changing main speed at analog signal input
I want to operate multiple inverters linked via a ratio setter, and also want to change each inverter's running frequency during operation.
Do you have a good idea to do this?
- Category :
-
Answer
To change the running frequency while the frequency command is input to the terminal 2, adjust the parameters in the following steps:
1. Change Pr.77 to "2".
2. Adjust the running frequency with Pr.903.
3. After adjustment, return Pr.77 to the original value.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500