• No : 22156
  • Release Date : 2018/08/27 16:41
  • Update : 2020/04/10 16:08
  • Print

Measurable minimum voltage (ME96SS series).

What is the Measurable minimum voltage?
Category : 

Answer

In case of the input voltage of less than 11 V, the measurement values are as follows:
 Voltage: 0 V, Power supply: 0 W, Reactive power: 0 var, Apparent power: 0 VA, and Power factor: 1.
Product Name
Electronic Multi-Measuring Instrument
Series
ME96SS series