• No : 22462
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/18 15:51
  • Print

Combination of the MELSEC iQ-R series inter-module synchronization function and another network synchronous communication function

Can I use the MELSEC iQ-R series inter-module synchronization function together with another network synchronous communication function, such as the CC-Link IE Field Network synchronous communication function?
Category : 

Answer

You can use the MELSEC iQ-R series inter-module synchronization function together with the CC-Link IE Field Network
synchronous communication function.With the CC-Link IE Field Network synchronous communication function,
you can operate other slave stations connected in the same network synchronously in an inter-module synchronization
cycle of the MELSEC iQ-R series inter-module synchronization function.

Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series