• No : 22465
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/19 11:57
  • Print

Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed

How long is the overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module?
Category : 

Answer

When the block number of the file register (R) is saved and stored, the overhead time becomes 35.9 [us].
When the number of the file register is not saved or stored, the overhead time becomes 18.6 [us].
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series