• No : 22499
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 12:14
  • Print

Overhead time before and after the startup of an interrupt program with a MELSEC iQ-R series CPU module

How long is the overhead time before and after the startup of an interrupt program with a MELSEC iQ-R series CPU module?
Category : 

Answer

Although it depends on interrupt factors, the overhead time before startup becomes 10.8 to 23.8 [us]
and the time after startup becomes 6.5 to 17.4 [us].

Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series