• No : 22869
  • Release Date : 2018/09/03 17:30
  • Print

Local device comments

Is it possible to read local device comments if comments are written to the CPU module?
Category : 

Answer

Local device comments can be read if the comment file in which the local device comments are stored is written to the CPU module.
Product Name
Engineering Software
Series
Software Package (GPP function)