• No : 22881
  • Release Date : 2018/09/03 17:30
  • Print

Using GX Logviewer's realtime monitor function on multiple personal computers

Is it possible to use the realtime monitor function of GX Logviewer on multiple personal computers?
Category : 

Answer

Up to two realtime monitor windows can be used for monitoring.
If each of two personal computers monitors one monitor window, two personal computers can be connected.
If a single personal computer monitors two windows, one personal computer can be connected.
Product Name
Engineering Software
Series
Software Package (other functions)