• No : 22941
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/25 09:58
  • Print

Displaying comments in GX Works2

How can I display comments in the ladder editor (circuit) of GX Works2?
Category : 

Answer

Select [View] -> [Comment] from the menu to display comments.
You can display local comments with the following procedure.

(1) Select [Tool] -> [Options] from the menu to open the Option window.
(2) Select [Program Editor] -> [All Editors] -> [Device Comment] from the tree on the left of the window.
(3) In Reference/Reflection Target for Device Comment, select global comments 
     or local comments as the device comments of each program.
Product Name
Engineering Software
Series
Software Package (GPP function)