• No : 22949
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/25 11:05
  • Print

Device numbers set in the initial setting procedure registration window of the CC-Link remote device station

Do I have to change device numbers of Initial data processing request flag (RX18) and others for each station number in the initial setting procedure registration window of the remote device station?
Category : 

Answer

You do not have to change the device numbers for each station number in the initial setting procedure registration window.

Example) When the AJ65SBT2B-64AD has been connected to the station numbers 1 and 2 In the initial setting procedure
                 registration window, set RX18 for Initial data processing request flag of both the station numbers 1 and 2.
Product Name
Engineering Software
Series
Software Package (GPP function)