• No : 22964
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/25 13:16
  • Print

Difference between QJ61BT11 and QJ61BT11N

What are the differences between QJ61BT11 and QJ61BT11N?
Category : 

Answer

QJ61BT11N supports Version 2 (expanded cyclic setting), the setting for refreshing/forced clearing a slave station data when the switch on a programmable controller CPU is set to STOP, and other functions.

For more details, refer to the following manual.
 - CC-Link System Master/Local Module User's Manual
   Appendix 5 Difference from traditional modules
   Appendix 5.2 Precautions when replacing a QJ61BT11 with a QJ61BT11N
Product Name
Network Related Products
Series
CC-Link