• No : 23085
  • Release Date : 2018/09/03 17:31
  • Print

Differences between CC-Link IE Control Network and CC-Link IE Field Network

What are the differences between the CC-Link IE Control Network and CC-Link IE Field Network?
Category : 

Answer

The CC-Link IE Control Network is a high-capacity controller network whose maximum number of link points is 128k words. The CC-Link IE Field Network is an all-around network that integrates the controller distributed control, I/O control, safety control, and motion control. The maximum number of link points is 16K words.
Product Name
Network Related Products
Series
CC-Link IE Field Network