FAQ
>
Robots
>
Industrial/Collaborative Robots-MELFA
>
Ceiling mounted, holizontal type robot
>
In automatic drive mode, the system does not start up or the robot stops during automatic drive.
Back
No : 23171
Release Date : 2018/09/07 16:09
Update : 2018/10/03 14:48
Print
In automatic drive mode, the system does not start up or the robot stops during automatic drive.
•In automatic drive mode the system does not start up even if a startup signal is input.
•The robot stops during automatic drive.
Category :
FAQ
>
Robots
>
Industrial/Collaborative Robots-MELFA
>
Vertical type robot
FAQ
>
Robots
>
Industrial/Collaborative Robots-MELFA
>
Horizontal type robot
FAQ
>
Robots
>
Industrial/Collaborative Robots-MELFA
>
Ceiling mounted, holizontal type robot
Answer
Cause:
A stop signal(STOP/STOP2/SKIP) is being input from an external source.
The operating right is not given.(IOENA parameters settings/exclusive input and output).
An error is occurring.
A start signal(START) has not been input.
The slot attribute settings are not set to START.
The program's operation commands have not been executed.
Measures:
Check for a stop/startup signals and check the operation rights.
Check the attributes of the program.
With the robot stopped, check the status of the operation program's execution.
If an error message is occurring please cancel it.
Product Name
Industrial Robots MELFA
Series
FR SeriesF Series