• No : 23172
  • Release Date : 2018/09/07 16:09
  • Print

The position becomes offset.

•The position becomes offset during automatic drive.
•The position becomes offset after moving the equipment.
Category : 

Answer

Cause:

  • Program error (arithmetic processing, etc.).
  • Teaching operation error.
  • Peripheral equipment is offset.
  • There is a setting error in the origin position data.
  • The origin position data has been lost(battery life, etc.).
  • Origin positions are offset(the arm was moved while the power supply was OFF, etc.)
  • Connecting parts have come loose.
  • Belt teeth have been skipped.
  • Increased backlash from the reduction gear.

Measures:

  • Check the positioning data in the area where the positioning has become offset.
  • Check the peripheral equipment and the robot's connecting parts(hand, robot installation section, etc.)
  • Check the remaining time on the robot battery's life.
  • Check the position of the origin positions.
  • Check the condition of the belt.
  • Check whether there is any nearby interference, etc.

Product Name
Industrial Robots MELFA
Series
FR Series
F Series