• No : 23177
  • Release Date : 2018/09/07 16:09
  • Print

The hand does not move properly (Electric operated hand).

The hand does not move properly
The hand operation screen is not displayed on the TB.
(Electric operated hand)
Category : 

Answer

Cause:

  • Wire breakage on the hand signal line.
  • The electronic hand controller(manufactured by TAIYO Ltd.) has failed.
  • Faulty connection in the cables that run between devices.
  • The software version on the TB and robot controller is not compatible with the electric operated hand.
  • The user is trying to use the electric operated hand on a model that is not compatible with the electric operated hand.

Measures:

  • Check the connections.
  • Check the condition of the hand input/output signal.
  • Check the mating condition of the cables that run between devices.
  • Check whether the software version is compatible or not.
  • Check the model compatibility.

Product Name
Industrial Robots MELFA
Series
FR Series
F Series