• No : 23240
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

How can I select a thermal load relay when it is installed in the deltaphase?
Category : 

Answer

When installing a thermal load relay in the delta phase and detectingphase current, you select a heater designation that can be set to 1 / √ 3times of the motor full-load current value and you set the current value ofcurrent knob to 1 / √ 3 times of the motor full-load current value.
Product Name
Motor Starters
Series
MS-T/N