• No : 23421
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:37
  • Print

Differences in the panel cutting dimensions from the GOT1000 series

Do the GOT1000 series and GOT2000 series have the same panel cutting dimensions when their models are the same in screen sizes?
Category : 

Answer

The GOT1000 series and GOT2000 series have the same panel cutting dimensions when their models are the same in screen sizes (excluding the GT25 open frame model).
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT
Series
GOT2000 Series