• No : 23479
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 18:10
  • Print

Screen switching in the screen gesture mode

What operation is performed when a screen switching occurs in the screen gesture mode?
Category : 

Answer

When a screen switching occurs in the screen gesture mode, the following operation is performed.

・ When the screen is being touched
 After you release the finger, the screen is switched and the screen gesture mode is canceled.
・ When the screen is not being touched
 The screen is switched immediately and the screen gesture mode is canceled.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series