You can cancel the screen gesture mode by the following methods.
・ Touch the screen gesture mode selector switch (key code: FF90).
・ Touch the full scale display (100%) switch (key code: FF91).
・ Switch to the utility screen.
・ Switch to the base screen.
・ Authorize VCN client when the GOT remote access function (VNC server function) is used.
・ Disable the authorization of the GOT network interaction function.
* Place the screen gesture mode selector switch outside the screen gesture active area.
* The full scale display (100%) switch is supported by GT Designer3 (GOT2000) Version 1.105K or later.
* The GOT network interaction function is supported by GT Designer3 (GOT2000) Version 1.144A or later.