• No : 23549
  • Release Date : 2018/09/14 15:07
  • Print

CC-Link IE Field Network Basic connection of the rugged model

Answer

The rugged model supports the CC-Link IE Field Network Basic connection.

Both Ethernet interface Port1 and Port2 are connectable to controllers that support the Ethernet and CC-Link IE Field Network Basic connections.
The GOT2000 series operates as a slave station and is connectable to controllers that operate as a master station.
(Supported by the RJ-45 connector (Port1, Port2))
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model, GOT function (communication)
Series
GOT2000 Series