• No : 23631
  • Release Date : 2018/09/14 15:10
  • Print

Servo motor does not rotate when the command pulse is input.

Servo motor does not rotate when the command pulse is input from the positioning module.
Category : 

Answer

The pulse train form outputted with the controller and the setting of servo amplifier (command pulse input form) may differ.
Check the parameter settings. (MR-J4-A: [Pr.PA13])

For the other causes, refer to “No Motor Rotation”, etc. of MR Configurator2 (servo setup software) to investigate. (* Some models are not supported.)

Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MELSERVO Others